Blog : Smart Connections
-
Office & Enterprise
Benefits of MPTL termination in enterprise
Network convergence in intelligent buildings brings more end devices such as Wireless Access Points, IP cameras and digital signage onto the LAN. Some located in high places are directly connected onto the horizontal network using a Modular Plug Terminated Link (MPTL) connection. But what is MTPL and how does it differ from the traditional Permanent Link method of installation?
-
Office & Enterprise
Overcoming challenges in scaling up networks
Today, it is more important than ever that networks can scale up easily, with regards to footprint as well as number of users. One approach to making LAN scalability in critical environments easy is following a Fibre To The Office (FTTO) solution.
-
Office & Enterprise
A closer look at Cybersecurity and LANs
As businesses and economies become more dependent on connectivity, they also become more vulnerable to cybercrime. Intelligent system features help increase network security. Find out how a Fibre to the Office (FTTO) solution offers a high level of built-in protection.
-
Industrial
What could IEC 61850 mean for your network?
Easier management and monitoring of smart grids– but keep an eye on compliance
-
Office & Enterprise
What could Wi-FI 6 mean for your LAN?
When making the move to Wi-Fi 6 - the next generation of the 802.11 WLAN standard – there are a few things that you’ll need to consider. Learn more in the Nexans Blog Post.